About this task
To install an NSW8000 Series Sensor, complete the following steps:
Procedure
- Select a mounting location for the sensor. Refer to the job site plans and the NSW8000 Series Wireless Network Sensors Installation Guide (LIT-12014419).
-
Set the NSW8000 Sensor DIP switches as shown in the following table.
Table 1. NSW Sensor DIP switch DIP switch Setting Mode Mesh Area Set to 0 Zone Set according to application requirements MS/TP Address Match the MS/TP address of the associated device (FEC/IOM/VMA16) PAN OFFSET Match the PAN OFFSET of the associated ZFR Pro Coordinator and ZFR Pro Routers Power OFF - Install two AA alkaline batteries (supplied) into the battery compartment on the back of the sensor. Ensure that you install the batteries in the correct polarity.
-
Secure the sensor to its mounting base. Keep the power off until the wireless
field bus system is ready to be commissioned.
Repeat these steps for each additional zone sensor.