Selecting a PAN OFFSET for a wireless network - Facility Explorer - LIT-12013796 - Wireless Device - WRG1830/ZFR183x Pro Series

WRG1830/ZFR183x Pro Series Wireless Field Bus for Facility Explorer Systems Technical Bulletin

Product
Document number
LIT-12013796
Revision date
2025-02-07
Product status
Active

When selecting a PAN OFFSET for a wireless network, keep these points in mind:

  • Set all devices within one wireless mesh network to the same PAN OFFSET.
  • Select PAN OFFSETs that are unique for the site.
Important: To avoid interference, assign a unique PAN OFFSET to each wireless network in a building. Using a unique PAN OFFSET is particularly important if you have PANs on adjacent floors of a building.
Important: Do not use the same PAN OFFSET on multiple wireless networks in a building, even if the transmit distances do not overlap.