Guidelines for locating ZFR Pro Series system components - Facility Explorer - LIT-12013796 - Wireless Device - WRG1830/ZFR183x Pro Series

WRG1830/ZFR183x Pro Series Wireless Field Bus for Facility Explorer Systems Technical Bulletin

Product
Document type
Technical Bulletin
Document number
LIT-12013796
Revision date
2025-02-07
Product status
Active

Use the following information to determine the optimum location to mount the WRG Wireless Router Gateway, ZFR Pro Routers, and WRZ and NSW8000 Sensors and to estimate the number of additional repeaters required.

  • The cable that connects a WEFC or WRG to its associated ZFR can be up to 30 m (100 ft) long to allow for better placement of the router/coordinator in the space.
  • Every router/repeater should be within 75 m (250 ft) (recommended) of at least two other routers/repeaters that are part of the same network (PAN).
  • Best practice is to keep the entire network (PAN) contained within a single floor or wing.
  • Minimize the number of hops (Router to Router communication) to transmit a message to the coordinator.
  • Every WRZ Sensor should be located within 15 m (50 ft) (recommended) of at least two router/repeaters. WRZ Sensors only communicate directly with router/repeaters.
  • Every NSW8000 Sensor should be located within 46 m (150 ft) (recommended) of at least two router/repeaters. NSW8000 Sensors only communicate directly with router/repeaters.
  • For best sensing and control, follow the locations as outlined in General HVAC Wiring & installation Requirements when you determine the WRZ and NSW8000 Sensor locations.