Locations or applications that prohibit cellular telephones or Wi-Fi systems are unsuitable for the wireless BAS products. Do not use the wireless products in applications that cannot tolerate intermittent interference. Examples include the following:
- Critical control features would affect life safety or result in large monetary loss, including secondary (backup) life-safety applications.
- Data centers, production lines, or critical areas would be shut down.
- Loss of critical control would result from loss of data from humidity or temperature sensor communications. WRZ and NSW8000 Sensors report as infrequent as once every 15 minutes to conserve battery life. It may take up to 1 hour for the controller to detect the loss of a defective sensor.
- Operation of exhaust fans or Air Handling Units (AHUs) would impair a purge or pressurization mode.
- Missing monitored data of security points would invalidate reporting required by the customer.
- Government installations where U.S. General Service Administration security requirements are more stringent.