Applications for wireless - Facility Explorer - LIT-12013796 - Wireless Device - WRG1830/ZFR183x Pro Series

WRG1830/ZFR183x Pro Series Wireless Field Bus for Facility Explorer Systems Technical Bulletin

Product
Document type
Technical Bulletin
Document number
LIT-12013796
Revision date
2025-02-07
Product status
Active

The wireless products within a BAS system are ideal for any location where it is cost-prohibitive, difficult, or aesthetically unappealing to hardwire between BAS products. Examples of these locations include the following:

  • Office buildings, university campuses, educational facilities, correctional facilities, and other commercial structures with brick or solid concrete walls, ceilings, or both that impede hard-wired applications.
  • Office buildings, retail stores, and other commercial real estate where tenant turnover is frequent and temporary walls and ceilings are common.
  • Museums, historical buildings, atriums, and other sites where building aesthetics and historical preservation are important.
  • Stadiums, arenas, gymnasiums, convention centers, airports, zoos, and other locations with large, open spaces, wood veneer, or other decorative surfaces that present challenges to hardwiring.
  • Buildings with asbestos or other hazardous materials that must not be disturbed.
  • Buildings with occupants sensitive to business disruptions.
  • Locations with high labor costs.