Commission and verify the WEFC - Facility Explorer - LIT-12013796 - Wireless Device - WRG1830/ZFR183x Pro Series

WRG1830/ZFR183x Pro Series Wireless Field Bus for Facility Explorer Systems Technical Bulletin

Product
Document type
Technical Bulletin
Document number
LIT-12013796
Revision date
2025-02-07
Product status
Active

To commission and verify the WEFCs, refer to Table 1.

Table 1. WRG commissioning features

WRG1830

MAP Gateway

Point Checkout Supported Supported
Airflow Balancing Supported Supported
Box Flow Test Supported Supported
Create Report Supported Supported
Tailored Summaries Not supported See note
Live Trend Not supported See note
Note: Tailored summaries are not supported across wireless networks.