Appendix A - Wireless security - Facility Explorer - LIT-12013796 - Wireless Device - WRG1830/ZFR183x Pro Series

WRG1830/ZFR183x Pro Series Wireless Field Bus for Facility Explorer Systems Technical Bulletin

Product
Document type
Technical Bulletin
Document number
LIT-12013796
Revision date
2025-02-07
Product status
Active

The WRG1830/ZFR183x Pro Series Wireless Field Bus System is secure for the following reasons:

  • The ZFR183x mesh over-the-air communication uses AES128 bit security.
  • The ZFR183x mesh network coordinator manages when devices can be added to the network and is able to be software locked to prevent unauthorized access.
  • The WRG1830 Gateway utilizes secure boot upon initialization and connection to the Ethernet network.
  • The ZFR183x Pro Series Wireless Field Bus devices transmit data using several short proprietary messages that are collected and reconstructed at the destination. If a piece of the message is intercepted, it is indecipherable to the outside source.
  • The WRG1830 Gateway requires authentication for user access with an audit log to track log-ins and commands.
  • The WRG1830 Gateway Wi-Fi functionality allows access to the wireless network configuration, but it does NOT create a Wi-Fi hotspot to the Internet.