Verify communications between the Coordinator Radio and the WNC Gateway - Facility Explorer - LIT-12012397 - FX-ZFR1820-0 - FX-WNC1820-0B - FX-ZFR1822-0B - FX-WNC1820-0A - FX-ZFR1823-0 - FX-ZFR1821-0B - FX-ZFR1822-0 - FX-ZFR1821-0 - FX-WNC1800-0S - FX-WNC1823-0B - FX-WNC1823-0A - Bulb controller - FX-ZFR182x Pro Series Wireless Field Bus System

WNC1800/FX-ZFR182x Pro Series Wireless Field Bus System Quick Reference Guide

Product
Network and Communications > Wireless Devices > FX-ZFR182x Pro Series Wireless Field Bus System
Document number
LIT-12012397
Revision date
2019-03-22

On the WNC1800 Home Screen (Device List > WNC > WNC Home Page), check that Current Radio Reliability is Online. The PAN ID and Active Channel are also shown. The PAN ID on the coordinator is set using the DIP switches. The WNC Gateway reads this number and shows it on this screen. Manually adjust the Active Channel, if necessary.