Set the PAN IDs in Your FX-ZFR Pro Coordinator Radio - Facility Explorer - LIT-12012397 - FX-ZFR1820-0 - FX-WNC1820-0B - FX-ZFR1822-0B - FX-WNC1820-0A - FX-ZFR1823-0 - FX-ZFR1821-0B - FX-ZFR1822-0 - FX-ZFR1821-0 - FX-WNC1800-0S - FX-WNC1823-0B - FX-WNC1823-0A - Bulb controller - FX-ZFR182x Pro Series Wireless Field Bus System

WNC1800/FX-ZFR182x Pro Series Wireless Field Bus System Quick Reference Guide

Product
Network and Communications > Wireless Devices > FX-ZFR182x Pro Series Wireless Field Bus System
Document number
LIT-12012397
Revision date
22/03/2019

Set the PAN ID DIP switches on the FX-ZFR Pro Coordinator Radio:

Notes:

  • Select PAN Addresses that are unique within the site.
  • All devices on the wireless network need to have the same PAN Offset.
  • Once the PAN has been selected and other devices start to join the network, do not change the PAN switches to another value and then back again. Changing the PAN switches causes that device to clear its network information, resulting in abandoned children. This can lead to duplicate network (short) addresses and controller online/offline toggling.
    Figure 1. Sample DIP switch settings

    Figure 2. TEC network setup and configuration menu