Configuring an FX Supervisory Controller - Facility Explorer - LIT-12012397 - FX-ZFR1820-0 - FX-WNC1820-0B - FX-ZFR1822-0B - FX-WNC1820-0A - FX-ZFR1823-0 - FX-ZFR1821-0B - FX-ZFR1822-0 - FX-ZFR1821-0 - FX-WNC1800-0S - FX-WNC1823-0B - FX-WNC1823-0A - Bulb controller - FX-ZFR182x Pro Series Wireless Field Bus System

WNC1800/FX-ZFR182x Pro Series Wireless Field Bus System Quick Reference Guide

Product
Network and Communications > Wireless Devices > FX-ZFR182x Pro Series Wireless Field Bus System
Document number
LIT-12012397
Revision date
2019-03-22

No manual configuration of the FX Supervisory Controller is necessary. As long as the WNC Enable/Disable Routing parameter is set to Enabled, you can use the existing process to discover the WEPCs as any other BACnet over IP device. Furthermore, you can use The FX Workbench JCI BACnet Import manager on the wireless devices.