Configure the WNC Gateway - Facility Explorer - LIT-12012397 - FX-ZFR1820-0 - FX-WNC1820-0B - FX-ZFR1822-0B - FX-WNC1820-0A - FX-ZFR1823-0 - FX-ZFR1821-0B - FX-ZFR1822-0 - FX-ZFR1821-0 - FX-WNC1800-0S - FX-WNC1823-0B - FX-WNC1823-0A - Bulb controller - FX-ZFR182x Pro Series Wireless Field Bus System

WNC1800/FX-ZFR182x Pro Series Wireless Field Bus System Quick Reference Guide

Product
Network and Communications > Wireless Devices > FX-ZFR182x Pro Series Wireless Field Bus System
Document type
Reference Guide
Document number
LIT-12012397
Revision date
22/03/2019

Refer to the WNC Gateway Quick Start Guide (Part No. 24-10737-105) for instructions on initial access to the WNC Gateway through a supported browser on either a PC or a mobile device. From the Device List, choose the WNC Gateway.

Note: The UI shows wireless signal strength of the devices connected to the WNC Gateway as well as any current alarms on the devices.