Complete the network setup - Facility Explorer - LIT-12012397 - FX-WNC1800-0S - FX-WNC1820-0A - FX-WNC1820-0B - FX-WNC1823-0A - FX-WNC1823-0B - FX-ZFR1820-0 - FX-ZFR1821-0 - FX-ZFR1821-0B - FX-ZFR1822-0 - FX-ZFR1822-0B - FX-ZFR1823-0 - Bulb controller - FX-ZFR182x Pro Series Wireless Field Bus System

WNC1800/FX-ZFR182x Pro Series Wireless Field Bus System Quick Reference Guide

Product
Network and Communications > Wireless Devices > FX-ZFR182x Pro Series Wireless Field Bus System
Document type
Reference Guide
Document number
LIT-12012397
Revision date
22/03/2019

On the Network Setup Screen shown below, the Wireless Field Bus Network address, BACnet® Device Object Identifier, and the BACnet IP Network address must be unique. One simple way to make the Wireless Field Bus Network address, BACnet Device Object Identifier, and the BACnet IP Network address is unique is to set it to the PAN ID of the attached coordinator. Other methods can also be used if appropriate for the site.

If you add the WNC Gateway and associated devices to a network that has a Supervisory Controller, you must set the Enable/Disable Routing field on the WNC Home Page to Enabled.

Note: Once you make these changes, you must change the Commit Changes and Reset field to True; then the WNC Gateway resets and comes up using the new settings.