Repair information - Facility Explorer - LIT-12012378 - FX-ZFR1820-0 - FX-WNC1820-0B - FX-ZFR1822-0B - FX-WNC1820-0A - FX-ZFR1823-0 - FX-ZFR1821-0B - FX-ZFR1822-0 - FX-ZFR1821-0 - FX-WNC1800-0S - FX-WNC1823-0B - FX-WNC1823-0A - Bulb controller - FX-ZFR182x Pro Series Wireless Field Bus System

WNC1800/FX-ZFR 182x Pro Series Wireless Field Bus System Product Bulletin

Product
Network and Communications > Wireless Devices > FX-ZFR182x Pro Series Wireless Field Bus System
Document number
LIT-12012378
Revision date
22/03/2019

If an FX-ZFR Pro Wireless Field Bus System component fails to operate within its specifications, replace the unit. For a replacement FX-ZFR Pro Series System component, contact the nearest Johnson Controls representative.

Table 1. FX-ZFR Pro Wireless Field Bus System components
Product code number Product description
FX-WNC1820-0A The FX-WNC1820-OA kit is comprised of the following components:
  • WNC Gateway and mounting base with 110/220 VAC Power Supply

  • The FX-ZFR1820 Pro Coordinator Radio with 3-Foot RJ-12 connecting cable

  • Box mount for FX-ZFR1820 Pro Coordinator Radio

FX-WNC1823-0A The FX-WNC1823-OA kit is comprised of the following components:
  • WNC Gateway and mounting base with 110/220 VAC Power Supply

  • The FX-ZFR1823 Pro Coordinator Radio with 10-Foot RJ-12 connecting cable

  • Mounting screws for FX-ZFR1823 Pro Coordinator Radio

Note: A field-provided ceiling clip is required to mount the FX-ZFR1823 Pro Coordinator Radio below grid ceilings.
FX-ZFR1821-0B The FX-ZFR1821-0B kit is comprised of the following components:
  • FX-ZFR1821 Pro Router, EMT mount, with 3-Foot RJ-12 connecting cable

  • 24 VAC to 15 VDC power supply for the router

  • Box mount for FX-ZFR1821 Pro Router

Note: Use the FX-ZFR1821 EMT mount repeater for above the ceiling mounting.

Use the alternative FX-ZFR1822 Pro Router for flush wall-mount or below the ceiling-mount applications. A field-provided ceiling clip is required to mount the FX-ZFR1822 Pro Router below grid ceilings.

FX-ZFR1822-0B The FX-ZFR1822-0B kit is comprised of the following components:
  • FX-ZFR1822 Pro Router, wall-mount, with 10-Foot RJ-12 connecting cable

  • 24 VAC to 15 VDC power supply for the router.

  • Drywall-mounting hardware (ceiling clips not provided due to variety of ceiling types)

Note: Use the FX-ZFR1822 Pro Router for flush wall-mount or below the ceiling-mount applications. A field-provided ceiling clip is required to mount the FX-ZFR1822 Pro Router below grid ceilings.Use the alternative FX-ZFR1821 EMT mount repeater for above the ceiling mounting.
FX-ZFR1821-0 The FX-ZFR1821-0 kit is comprised of the following components:
  • FX-ZFR1821 Pro Router, EMT mount, functions with BACnet WEPCs and FX-WRZ Series Sensors

  • Box mount for FX-ZFR1821

Note: Use the FX-ZFR1821 EMT mount repeater for above the ceiling mounting.

Use the alternative FX-ZFR1822 Pro Router for flush wall-mount or below the ceiling-mount applications. A field-provided ceiling clip is required to mount the FX-ZFR1822 Pro Router below grid ceilings.

FX-ZFR1822-0 The FX-ZFR1822-0 kit is comprised of the following components:
  • FX-ZFR1822 Pro Router, wall-mount, 10 mW Transmission Power; functions with BACnet FX-PCGs, FX-PCXs, FX-PCVs, and FX-WRZ Series Sensors

  • Drywall-mounting hardware (ceiling clips not provided due to variety of ceiling types)

Note: Use the FX-ZFR1822 Pro Router for flush wall-mount or below the ceiling-mount applications. A field-provided ceiling clip is required to mount the FX-ZFR1822 Pro Router below grid ceilings.Use the alternative FX-ZFR1821 EMT mount repeater for above the ceiling mounting.
FX-WNC1820-0B The FX-WNC1820-OB kit is comprised of the following components:
  • WNC Gateway and mounting base with 24 VAC Power Supply and WNC power adapter cable

  • FX-ZFR1820 Pro Coordinator Radio with 3-Foot RJ-12 connecting cable

  • Box mount for FX-ZFR1820 Pro Coordinator Radio

FX-WNC1823-0B The FX-WNC1823-OB kit is comprised of the following components:
  • WNC Gateway and mounting base with 24 VAC Power Supply and WNC power adapter cable

  • FX-ZFR1823 Pro Coordinator Radio with 10-Foot RJ-12 connecting cable

  • Mounting screws for FX-ZFR1823 Pro Coordinator Radio

Table 2. Related Field Controllers and Sensors
Product code number Product Description
TEC30xx-0x-000 For information on Wireless TEC3000 Models, refer to the TEC3000 Series Wireless, Stand-Alone, and Field-Selectable BACnet® MS/TP or N2 Networked Thermostat Controllers Product Bulletin (LIT-12011954) for ordering information. This document describes the different models and links to further information such as installation instructions.
FX-PCAxxxx, FX-PCGxxxx, FX-PCXxxxx, FX-PCVxxxx For information on Wireless Enabled Field Controllers, refer to the FX-PC Series Programmable Controllers and Related Products Product Bulletin (LIT-12011657). This document describes the different models and links to further information such as installation instructions.
FX-WRZ-xxxx For information on FX-WRZ Series Room sensors, refer to the FX-WRZ Series Wireless Room Sensors Product Bulletin (LIT-12011687). This document describes the different models and links to further information such as installation instructions.
Table 3. Accessories
Product code number Product description
FX-ZFRCBL-0 Wire Harness with Connectors for use with FX-ZFR182x-x Router for Wireless Field Bus. Allows FX-ZFR1821 or FX-ZFR1822 Pro Router to function with FX-PCG1620 controller; and with FX-PCG1610, FX-PCV1610, or FX-PCV1620 controllers in conjunction with NS Series Sensors, FX-BTCVT-1 Bluetooth Converter, or FX-DIS1710 Local Controller Display.
FX-ZFRUSBHA-0 Universal Serial Bus (USB) Dongle with FX-ZFR Driver provides a wireless connection through the CCT to allow wireless commissioning of the wirelessly enabled FX-PCG, FX-PCX, and FX-PCV Series Field Controllers. Also used for the ZFR Checkout Tool (ZCT) in CCT.
FX-ZFRWallCover The FX-ZFRWallCover is an optional accessory of the WNC1800/FX-ZFR1820 Series System and is meant to enable mounting of the FX-ZFR1822 Pro Router or FX-ZFR1823 Pro Coordinator Radio, to be wall-mounted to an existing double-gang electrical box.
FX-WRZSST-120 Optional Wireless Sensing System Tool to be used with an FX-WRZ Series Sensor to indicate wireless signal strength between potential locations of FX-ZFR1800 System devices.
1.5 VDC, AA Alkaline Battery Replacement Battery for FX-WRZ Series Sensors (Purchase Locally)