If an FX-ZFR Pro Wireless Field Bus System component fails to operate within its specifications, replace the unit. For a replacement FX-ZFR Pro Series System component, contact the nearest Johnson Controls representative.
Product code number | Product description |
---|---|
FX-WNC1820-0A | The FX-WNC1820-OA kit is comprised of the following components:
|
FX-WNC1823-0A | The FX-WNC1823-OA kit is comprised of the following components:
Note: A field-provided ceiling clip is required to mount the FX-ZFR1823 Pro Coordinator Radio below grid ceilings.
|
FX-ZFR1821-0B | The FX-ZFR1821-0B kit is comprised of the following components:
Note: Use the FX-ZFR1821 EMT mount repeater for above the ceiling mounting.
Use the alternative FX-ZFR1822 Pro Router for flush wall-mount or below the ceiling-mount applications. A field-provided ceiling clip is required to mount the FX-ZFR1822 Pro Router below grid ceilings. |
FX-ZFR1822-0B | The FX-ZFR1822-0B kit is comprised of the following components:
Note: Use the FX-ZFR1822 Pro Router for flush wall-mount or below the ceiling-mount applications. A field-provided ceiling clip is required to mount the FX-ZFR1822 Pro Router below grid ceilings.Use the alternative FX-ZFR1821 EMT mount repeater for above the ceiling mounting.
|
FX-ZFR1821-0 | The FX-ZFR1821-0 kit is comprised of the following components:
Note: Use the FX-ZFR1821 EMT mount repeater for above the ceiling mounting.
Use the alternative FX-ZFR1822 Pro Router for flush wall-mount or below the ceiling-mount applications. A field-provided ceiling clip is required to mount the FX-ZFR1822 Pro Router below grid ceilings. |
FX-ZFR1822-0 | The FX-ZFR1822-0 kit is comprised of the following components:
Note: Use the FX-ZFR1822 Pro Router for flush wall-mount or below the ceiling-mount applications. A field-provided ceiling clip is required to mount the FX-ZFR1822 Pro Router below grid ceilings.Use the alternative FX-ZFR1821 EMT mount repeater for above the ceiling mounting.
|
FX-WNC1820-0B | The FX-WNC1820-OB kit is comprised of the following components:
|
FX-WNC1823-0B | The FX-WNC1823-OB kit is comprised of the following components:
|
Product code number | Product Description |
---|---|
TEC30xx-0x-000 | For information on Wireless TEC3000 Models, refer to the TEC3000 Series Wireless, Stand-Alone, and Field-Selectable BACnet® MS/TP or N2 Networked Thermostat Controllers Product Bulletin (LIT-12011954) for ordering information. This document describes the different models and links to further information such as installation instructions. |
FX-PCAxxxx, FX-PCGxxxx, FX-PCXxxxx, FX-PCVxxxx | For information on Wireless Enabled Field Controllers, refer to the FX-PC Series Programmable Controllers and Related Products Product Bulletin (LIT-12011657). This document describes the different models and links to further information such as installation instructions. |
FX-WRZ-xxxx | For information on FX-WRZ Series Room sensors, refer to the FX-WRZ Series Wireless Room Sensors Product Bulletin (LIT-12011687). This document describes the different models and links to further information such as installation instructions. |
Product code number | Product description |
---|---|
FX-ZFRCBL-0 | Wire Harness with Connectors for use with FX-ZFR182x-x Router for Wireless Field Bus. Allows FX-ZFR1821 or FX-ZFR1822 Pro Router to function with FX-PCG1620 controller; and with FX-PCG1610, FX-PCV1610, or FX-PCV1620 controllers in conjunction with NS Series Sensors, FX-BTCVT-1 Bluetooth Converter, or FX-DIS1710 Local Controller Display. |
FX-ZFRUSBHA-0 | Universal Serial Bus (USB) Dongle with FX-ZFR Driver provides a wireless connection through the CCT to allow wireless commissioning of the wirelessly enabled FX-PCG, FX-PCX, and FX-PCV Series Field Controllers. Also used for the ZFR Checkout Tool (ZCT) in CCT. |
FX-ZFRWallCover | The FX-ZFRWallCover is an optional accessory of the WNC1800/FX-ZFR1820 Series System and is meant to enable mounting of the FX-ZFR1822 Pro Router or FX-ZFR1823 Pro Coordinator Radio, to be wall-mounted to an existing double-gang electrical box. |
FX-WRZSST-120 | Optional Wireless Sensing System Tool to be used with an FX-WRZ Series Sensor to indicate wireless signal strength between potential locations of FX-ZFR1800 System devices. |
1.5 VDC, AA Alkaline Battery | Replacement Battery for FX-WRZ Series Sensors (Purchase Locally) |