Locations or applications that prohibit cellular telephones or Wi-Fi systems are unsuitable for the wireless FX-PC products. Examples include the following locations or applications:
- Operating rooms or radiation therapy rooms
- Validated environments
- UL 864 applications
- Department of Defense applications requiring DIACAP certification (for example, military bases and military hospitals)
Do not use the wireless FX-PC products in applications that cannot tolerate intermittent communication interference, or where the following may occur:
- Critical control features would impact life-safety or result in large monetary loss, including secondary (backup) life-safety applications
- Data centers, production lines, or critical areas would be shut down
- Loss of critical control would result from loss of data from humidity or temperature sensor communications
- Operation of exhaust fans or Air Handling Units (AHUs) would impair a purge or pressurization mode
- Missing data would invalidate reporting required by the customer
- Security points are monitored