Document introduction - Facility Explorer - Johnson Controls - Metasys - LIT-12014282 - TAD0471-0 - TAD0701-0 - TAD1001-0 - Field Device - Touch Advanced Display

Touch Active Display (TAD) Protocol Implementation Conformance Statement

Product
Controls > Control Displays > Touch Advanced Display
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12014282
Revision date
2023-05-08
Product status
Active

This document contains the Protocol Implementation Conformance Statement (PICS) and BACnet® Interoperability Building Blocks (BIBBs) for the Touch Active Display (TAD), as required by the ANSI/ASHRAE Standard 135 for BACnet protocol.

The PICS is a written document created by the manufacturer of a device to identify the particular options specified in the BACnet standard and implemented in the device.

BIBBs are collections of one or more BACnet services. This document includes a listing of the BIBBs currently supported by the TAD.