Character sets supported - Facility Explorer - Johnson Controls - Metasys - LIT-12014282 - TAD0471-0 - TAD0701-0 - TAD1001-0 - Field Device - Touch Advanced Display

Touch Active Display (TAD) Protocol Implementation Conformance Statement

Product
Controls > Control Displays > Touch Advanced Display
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12014282
Revision date
2023-05-08
Product status
Active

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

ISO 10646 Unicode Transformation Format-8 (UTF-8)

ISO 10646 Universal Character Set-2 (UCS-2)

IBM®/ Microsoft® Double-Byte Character Set (DBCS)

ISO 10646 (UCS-4)

ISO 8859-1

Japanese Industrial Standard (JIS) X 0208