Object type | Create or delete | Optional properties | Proprietary properties | Writable properties |
---|---|---|---|---|
Device | No |
OBJECT_IDENTIFIER NUMBER_OF_APDU_RETRIES APDU_TIMEOUT OBJECT_NAME (max 64 chars) LOCATION (max 64 chars) DESCRIPTION (max 64 chars) MAX_INFO_FRAMES MAX_MANAGER |
Note: The TAD
supports persistence of Device Object writable properties across power cycles.
Some of these properties, such as OBJECT_IDENTIFIER, APDU_TIMEOUT, OBJECT_NAME,
DESCRIPTION, MAX_INFO_FRAMES and MAX_MANAGER, are exposed as protocol parameters in the HMI programming
software. The HMI programming software does not reflect current settings if a
property is overwritten.