BACnet Interoperability Building Blocks (BIBBs) (Annex K) - Facility Explorer - Johnson Controls - Metasys - LIT-12014282 - TAD0471-0 - TAD0701-0 - TAD1001-0 - Field Device - Touch Advanced Display

Touch Active Display (TAD) Protocol Implementation Conformance Statement

Product
Controls > Control Displays > Touch Advanced Display
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12014282
Revision date
2023-05-08
Product status
Active
The following table lists all BIBBs that are supported.
Table 1. BACnet B-BC BIBBs Support
BIBB Name (A = Initiates and B = Executes) Designation

Device Management - Dynamic Device Binding - A

DM-DDB-A

Device Management - Dynamic Device Binding - B

DM-DDB-B

Device Management - Device Object Binding - B

DM-DOB-B

Data Sharing - Read Property - A

DS-RP-A

Data Sharing - Read Property - B

DS-RP-B

Data Sharing - Read Property Multiple - A

DS-RPM-A

Data Sharing - Read Property Multiple - B

DS-RPM-B

Data Sharing - Write Property - A

DS-WP-A

Data Sharing - Write Property - B

DS-WP-B
Data Sharing - View - A DS-V-A
Data Sharing - Modify - A DS-M-A

Data Sharing - COV - A

DS-COV-A