BACnet Standardized Device Profile (Annex L) - Facility Explorer - Johnson Controls - Metasys - LIT-12014282 - TAD0471-0 - TAD0701-0 - TAD1001-0 - Field Device - Touch Advanced Display

Touch Active Display (TAD) Protocol Implementation Conformance Statement

Product
Controls > Control Displays > Touch Advanced Display
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12014282
Revision date
2023-05-08
Product status
Active

BACnet Operator Workstation (B-OWS)

BACnet Advanced Operator Workstation (B-AWS)

BACnet Operator Display (B-OD)

BACnet Building Controller (B-BC)

BACnet Advanced Application Controller (B-AAC)

BACnet Application Specific Controller (B-ASC)

BACnet Smart Sensor (B-SS)

BACnet Smart Actuator (B-SA)

Note: The implementation of the BACnet protocol in JMobile HMI software follows the B-OD device profile with the exception of AE-VN-A.