Ring manager IP network system - Facility Explorer - LIT-1901114 - Field Device - Ring Manager IP Network System

Ring Manager IP Network System for Facility Explorer Catalog Page

Brand
Facility Explorer
Product name
Ring Manager IP Network System
Document type
Catalog Page
Document number
LIT-1901114
Revision date
2023-10-02
Language
English

You can use the items described in this catalog page to set up an IP network that contains a variety of components from a variety of manufacturers. You can build a network in many different ways. The items described here are a select subset of what is available, but are included for the following reasons:

  • They can be used to build a complete network capable of supporting a large FX installation based on IP-enabled supervisory controllers and equipment controllers. The IP Network Wizard is a system design tool, and is provided to help you to select and configure components from this catalog page.
  • They are industrial grade components that are suitable to deploy in building management system environments.
  • They are interoperable with each other, with the vendor’s full line of networking equipment, and with the equipment from all other large manufacturers.
  • Johnson Controls' relationship with Cisco Systems enables access to a variety of technical solutions available worldwide.
  • They improve network convergence time compared to rings managed using Rapid Spanning Tree Protocol.