Selection charts - Facility Explorer - Metasys - LIT-1901096 - Field Device - Ring Manager IP Network System

Ring Manager IP Network System Catalog Page

Product name
Ring Manager IP Network System
Document type
Catalog Page
Document number
LIT-1901096
Revision date
2024-05-21
The part numbers listed in this section have been identified as the Cisco Systems kits that may be required for a ring manager enabled network based on specific network design and needs. For best practice, use the IP Network Wizard Tool to generate an estimated list of basic equipment.
Note: The parts listed in Table 1 make up a minimum ring manager configuration. You can add or select additional items in subsequent tables as alternative options if needed.
Table 1. Typical Cisco Systems part numbers for basic ring manager configuration
Cisco product code number Description
IE-2000-8TC-G-E

8-port managed network switch

  • Industrial-grade Ethernet switch
  • Fully managed, Layer 2/Layer 3 switch
  • 8 Fast Ethernet ports (10/100 Mbit/sec) for network access
  • 2 Gigabit Ethernet ports (1000 Mbit/sec) for uplink, optionally upgradeable to optical fiber
  • SD card slot and console port provide two options for switch configuration
  • Supports a wide range of security options, including access control lists (ACLs)
  • Supports MRP for redundant connectivity
  • Supports Rapid Spanning Tree Protocol (RSTP) for redundant connectivity
  • Cisco Description: IE 8 10/100,2 T/SFP, Base with 1588
PWR-IE50W-AC-IEC=

AC Power Module with IEC Plug and Right Angle Power Cord, 110 V

This is the power supply for the switch. It is designed for operation in all regions of the world. The power cord is for the region of the world that includes the United States and Canada.
Note: Additional wiring is needed to connect the power supply to the switch. Both the power supply and switch come with appropriate connectors, but you need to supply wire and prepare cabling in the field.
  • Includes Cisco Part Number: CAB-AC-RA
  • Cisco Descriptions: AC Power Module w/ IEC Plug; Power Cord, 110V, Right Angle
SD-IE-1GB

IE 1GB SD Memory Card for IE 2000, IE 4010

Use this SD card to provision the switch with the configuration file and operating system. If you use Cisco's Industrial Network Director (IND) to commission the switch, you do not require an SD card.

  • Cisco Description: IE 1GB SD Memory Card for IE 2000, IE 4010
CAB-CONSOLE-USB

Console Cable 6 ft. with USB Type A and mini-B

Optional cable used to connect to the IE 2000 switch console for local administration. To run a console session from the command-line interface, you also need to download a driver from Cisco. It is useful to have one cable per site for troubleshooting.

  • Cisco Description: Console Cable 6 ft. with USB Type A and mini-B
LIC-MRP-MULTI-MGR=

Cisco MRP Multi Domain MRP Manager

This license makes it possible to run up to three MRP rings on a single IE 2000 switch. The license is purchased once and lasts for the lifetime of the switch.

  • Cisco Description: Cisco MRP Multi Domain Manager Functionality
CON-SNT-IE20008E

SMARTnet support contract with a one-year term for IE-2000-8TC-G-E

Renewable SMARTnet contract enables Cisco Technical Assistance Center (TAC) support. This covers everything from phone support to equipment replacement. Each contract is tied to a specific switch based on the switch's serial number.​

  • Cisco Description: SNTC-8X5XNBD IE 8 10/100,2 T/SFP
Important: When you order a Cisco SMARTnet license, you must provide a contact name, email address and telephone number as part of the customer registration.

You can add the parts listed in the following table to a minimum ring manager configuration, or select them as alternative options. If you require a larger capacity switch, you can substitute items IE-2000-8TC-G-E and CON-SNT-IE20008E in Table 1 with the parts listed in the first two rows of Table 2.

Table 2. Optional: IE 2000 components
Cisco product code number Description
IE-2000-16TC-G-E

16-port managed network switch

This is the same as the IE-2000-8TC-G-E, except that has 16 ports for network access.

Note: If you substitute the IE-2000-8TC-G-E hardware, you must also substitute the support contract. See entry for code number CON-SNT-IE20001E.
  • Cisco Description: IE 16 10/100,2 FE SFP+2 T/SFP, Base with 1588
CON-SNT-IE20001E

SMARTnet support contract with a one-year term for IE-2000-16TC-G-E

Renewable SMARTnet contract enables Cisco TAC support. This covers everything from phone support to equipment replacement. Each contract is tied to a specific switch based on the switch's serial number.​

  • Cisco Description: SNTC-8X5XNBD IE 16 10/100,2 FE SF
Important: When you order a Cisco SMARTnet license, you must provide a contact name, email address and telephone number as part of the customer registration.
GLC-LX-SM-RGD=

1000Mbps Single Mode Rugged SFP

Single form-factor pluggable module for interfacing with fiber optic cable. Use this item to adapt the IE 2000 bundle for use with optical fiber.

Works with both single-mode and multi-mode fiber.

Provides extended reach of more than the 100 meters that is standard for Ethernet; the actual reach depends on the type of optical fiber used.

Note: Two SFPs are needed per optical fiber.
  • Cisco Description: 1000Mbps Single Mode Rugged SFP

If an IE 4010 aggregation switch is required by customer design for either aggregation or additional connection ports, order the parts listed in Table 3. The IE 2000 ring manager switches typically connect up through an aggregation switch such as the IE 4010 or equivalent.

Table 3. Optional: IE 4010 aggregation switch components
Cisco product code number Description
IE-4010-4S24P

IE 4010 network switch for aggregation

This switch is recommended as an aggregation switch for large networks. The purpose of an aggregation switch is to interconnect the access switches.

  • Cisco Description: IE 4010 4x 1G SFP, 24 10/100/1000 GE PoE LAN Base
CON-SNT-IE40104S

SMARTnet support contract with a one-year term for IE 4010 switch

Note: Use this item with an IE 4010 aggregation switch.

SMARTnet support contract with a one-year term Renewable SMARTnet contract enables Cisco TAC support. This covers everything from phone support to equipment replacement. Each contract is tied to a specific switch based on the switch's serial number.​

  • Cisco Description: SNTC-8X5XNBD IE 4010 4x 1G SFP, 24
Important: When you order a Cisco SMARTnet license, you must provide a contact name, email address and telephone number as part of the customer registration.
PWR-RGD-AC-DC-H

Power supply for IE 4010 network switch

Note: Use this item with an IE 4010 aggregation switch.

Power Supply for the IE 4010 Switch.

  • Cisco Description: IE 4010/5000 Hazloc Pwr Supply High AC/DC 85-264VAC/88-300VDC
Note: The power supply has screw terminals for connecting a power cord. A power cord is not included and must be obtained separately.
SD-IE-1GB

IE 1GB SD Memory Card for IE 2000, IE 4010

Use this SD card to provision the switch with the configuration file and operating system. If you use Cisco's Industrial Network Director (IND) to commission the switch, you do not require an SD card.

  • Cisco Description: IE 1GB SD Memory Card for IE 2000, IE 4010