You can connect IP-enabled controllers to the IE 3000 Series switch in many ways, because the IE 3000 Series is a fully-featured, managed switch. The following figure demonstrates one possible ring combination, and identifies the network components that you may require. Use this catalog page to identify ordering information for the items labeled as 2 and 4 in the following figure. For ordering of the other items, please refer to the respective IP Equipment Controller, Supervisory Controller, or Server catalog pages.
Label | Description |
---|---|
1 | Server |
2 |
Aggregation Switch If this functionality is not provided by an IT department, the IP Network Wizard tool guides you toward selection of either the Cisco IE 4010 or Cisco IE 3100. See Table 3 for the list of components required to install one of the Cisco IE switches as an aggregation switch. |
3 |
Access switch If this functionality is not provided by an IT department, the IP Network Wizard tool guides you to select an appropriate Cisco IE 3100 switch. Two models are available for you to purchase, one with 8 Ethernet ports for network access, the other with 18 ports. For the list of components related to the 8-port IE 3100, see Table 1. For information about the 18-port version, see Table 2. |
4 |
Supervisory device For more information about Metasys engines, refer to the Network Engines Product Bulletin (LIT-12012138) For more information about Facility Explorer controllers, refer to the FX80 Supervisory Controller Product Bulletin (LIT-12012250) and FX90 Supervisory Controller Product Bulletin (LIT-12014354) |
5 |
IP equipment or IP-enabled controllers arranged in a ring network For more information about Metasys IP equipment controllers refer to the Metasys CG, CV Equipment Controllers and XPM Expansion Modules Product Bulletin (LIT-12013105). For more information about Facility Explorer IP-enabled Equipment Controllers refer to the Facility Explorer CG, CV Series Equipment Controllers and XPM Expansion Modules Product Bulletin (LIT-12013225). |