Special tools needed - Facility Explorer - Part No. 24-10143-918 - FX-SC8XD485-0 - Bulb controller - RS-485 Option Module

RS-485 Option Module Installation Instructions

Product
Controls > Rs-485 Modules > RS-485 Option Module
Document number
Part No. 24-10143-918
Document revision
A
Revision date
2019-03-22

You need suitable tools and fasteners to mount and attach the unit to an already mounted FX80 controller. DIN-rail mounting of the controller and all its option modules is recommended.

A small flat-blade screwdriver is required to make wiring connections to RS-485 trunks.