Precautions - Facility Explorer - Part No. 24-10143-918 - FX-SC8XD485-0 - Bulb controller - RS-485 Option Module

RS-485 Option Module Installation Instructions

Product
Controls > Rs-485 Modules > RS-485 Option Module
Document number
Part No. 24-10143-918
Document revision
A
Revision date
2019-03-22

General precautions

Important: Remove all power to controller before attaching (plug in) or detaching (unplug) any option card module, to prevent possible equipment damage.
Important: Removal of the cover is not required. The option module contains no configurable or user-serviceable items (such as jumpers).

Static discharge precautions

Static charges produce voltages high enough to damage electronic components. The microprocessors and associated circuitry within the devices are sensitive to static discharge.

Important: Work in a static-free area. Discharge any static electricity you may have accumulated. Discharge static electricity by touching a known, securely grounded object. Do not handle the printed circuit board (PCB) without proper protection against static discharge. Use a wrist strap when handling PCBs. Secure the wrist strap clamp to earth ground.