The PCXs are expansion I/O modules with integral RS-485 MS/TP communications.
PCXs can serve in one of two capacities, depending on where they are installed in the control system. When installed on the Sensor Actuator (SA) Bus of PCA controllers, the PCXs expand the I/O interfaces of the controllers. When installed on the Field Controller (FC) Bus, PCXs can be used as I/O point multiplexors to support monitoring and control from a supervisory controller. The point multiplexor can also be useful for sharing points between other PC controllers on the FC Bus using peer-to-peer connectivity.
A full range of PCA models combined with the PCX models can be applied to a wide variety of building applications ranging from simple fan coil or heat pump control to advanced central plant management.