Setting up a local display - Facility Explorer - CH-PCA3613 - Field Device - FX-PCA36 Advanced Application Programmable Controller

PCA3613 Advanced Application Programmable Controller Installation Guide

Product
Controls > Programmable Controls > FX-PCA36 Advanced Application Programmable Controller
Document revision
E
Revision date
2020-11-11
docpartnumberlabel
Part No.
Part number
24-10143-1175

This PCA model does not have an integral display, but you can connect the controller to a FX-DIS1710 Local Controller Display. For detailed information about setting up and operating either an integral user interface or a remotely connected FX-DIS1710 display, refer to the FX-DIS Local Controller Display Technical Bulletin (LIT-12011666)