Firmware Package File - Facility Explorer - CH-PCA3613 - Field Device - FX-PCA36 Advanced Application Programmable Controller

PCA3613 Advanced Application Programmable Controller Installation Guide

Product
Controls > Programmable Controls > FX-PCA36 Advanced Application Programmable Controller
Document type
Installation Guide
Document revision
E
Revision date
2020-11-11
docpartnumberlabel
Part No.
Part number
24-10143-1175

The FX-FCP-0 equipment controller firmware package files are required for CCT to configure and commission the controllers. The firmware package files also allow you to upgrade an existing PCX to the latest firmware release available for that expansion module.

Beginning at CCT Release 13, the firmware package files are orderable separately; they are not included with CCT.

For additional information about the firmware package files, refer to the CCT Installation Instructions (LIT-12011259).