You commission BACnet MS/TP controllers with the (Controller Configuration Tool ) CCT software. Beginning at CCT Release 13, the firmware package files are orderable separately; they are not included with CCT. They are obtained from the Metasys software licensing portal, and are loaded and licensed on the computer/server that is running CCT. The controller can be connected through MAP 4.2+/BACnet Router (Mobile Access Portal (MAP) Gateway at version 4.2 or above). Refer to Controller Tool Help (LIT-12011147) for detailed information on commissioning field controllers. .