To mount a controller directly on a wall or other flat vertical surface, complete
the following steps:
Procedure
Pull the two bottom mounting clips outward and ensure they are
locked in the extended position.
Mark the mounting hole locations on the wall in either the
horizontal or vertical mounting position. Or hold the controller up to the wall
or surface in a proper mount position and mark the hole locations through the
mounting clips.
Drill holes in the wall or surface at the marked locations, and insert appropriate wall anchors in the holes (if necessary).
Hold the controller in place, and insert the screws through the mounting clips and into the holes (or anchors). Carefully tighten all of the screws.
Important: Do not overtighten the mounting screws. Overtightening the screws may damage the mounting clips.