Mounting Features and Dimensions - Facility Explorer - CH-PCA3613 - Field Device - FX-PCA36 Advanced Application Programmable Controller

PCA3613 Advanced Application Programmable Controller Installation Guide

Product
Controls > Programmable Controls > FX-PCA36 Advanced Application Programmable Controller
Document revision
E
Revision date
2020-11-11
docpartnumberlabel
Part No.
Part number
24-10143-1175

See Figure 1 for mounting dimensions in millimeters and inches. Inches are listed in parenthesis. Figure 1 also illustrates the DIN rail channel and the mounting clips in an extended position.

Figure 1. Back of Controller