The PCA3613 Advanced Application Programmable Controller is part of the Facility Explorer® Programmable Controller (FX-PC) family. The PCA36 controllers run pre-engineered and user-programmed applications and provides the inputs and outputs required to monitor and control a wide variety of HVAC and other facility equipment.
PCA36 controllers operate on an RS-485 BACnet® MS/TP Bus as BACnet Advanced Application Controllers (B-AACs) and integrate into Johnson Controls® and third-party BACnet systems.
controllers include an integral real-time clock, which enables the controllers to monitor and control schedules, calendars, and trends, and operate for extended periods of time as stand-alone controllers when offline from the system network.