Attribute |
VMA14xx |
FX-PCV1832 |
Implication |
---|---|---|---|
Network Sensors Supported |
TMZ Series Zone Sensors |
NS Series Network Sensors |
Replace TMZ with NS sensor. |
Wireless Sensors Supported |
TE-77 Wireless Room Sensor Transmitter/Receiver |
FX-WRZ7860 One-to-One Wireless Sensing System |
Replace TE-77 with FX-WRZ7860 One-to-One Wireless Sensing System. |
WRS-TTxx |
FX-WRZ7860 One-to-One Wireless Sensing System |
Replace WRS-TTxx with FX-WRZ7860 One-to-One Wireless Sensing System. |
|
Analog Sensors Supported |
TE-67 and TE-68 Series |
TE-77 and TE-68 Series |
Reusing sensors is possible. |
If you reuse a TE-67xx or TE-68xx Series sensor, be aware that the single setpoint or no setpoint models feature an LED, but the FX-PCG controller does not support the LED. As a result, you need to change the sensor's DIP switch settings as follows:
- If Temporary Occupied function is required for the application, set the DIP switch positions on the back of the sensor to down, up, and down (LED disabled, but Sensor and Push Button enabled).
- If Temporary Occupied function is
not required, set the DIP switch positions to down, down, and down
(LED and PB disabled). Figure 1. TE-67xx and TE-68xx Sensor DIP Switch Setting
Dual setpoint sensor models do not feature an LED, and as a result, you should not need to change the DIP switch settings.