- The FX-PCV1832 has a slightly larger footprint than the VMA14xx.
- Replacement in the same enclosure space is possible. However, it may be tight for some installations.
- The location of the retaining screw for the FX-PCV1832 controller is further away from the actuator shaft than on the VMA14xx.
Figure 1. Footprint considerations

|
Dimension |
VMA14xx |
FX-PCV1832 |
|---|---|---|
|
Height |
153 mm (6 in.) |
165 mm (6.5 in) |
|
Width |
102 mm (4 in.) |
125 mm (4.92 in.) |
|
Depth |
102 mm (4 in.) |
73 mm (2.9 in.) |