Zone bus considerations - Facility Explorer - LIT-12012045 - Bulb controller - Facility Explorer N2 Controller

Modernization Guide for N2 Controllers - Facility Explorer

Product
Network and Communications > N2 Controls > Facility Explorer N2 Controller
Document type
User Guide
Document number
LIT-12012045
Revision date
22/03/2019

VAV1xx controllers support a Zone Bus for optionally connecting TMZ Series network room sensors, TE-77 Series wireless temperature sensors and receivers, and M100C Series networked actuators. FX-PC controllers do not support the Zone Bus, and accordingly do not support these devices. Instead, FX-PC controllers feature a different technology bus called the Sensor Actuator (SA) bus for connecting NS Series Network Sensors and FX-PCX Series Expansion I/O Modules.

When using an FX-PC controller to replace a VAV1xx controller that uses a TMZ sensor, you must also replace the TMZ sensor with an NS Series Network Sensor. The NS sensor provides many of the same functions as the TMZ sensor, including zone temperature sensing, zone temperature setpoint adjustment, and LCD display. However, the NS sensor is housed in an enclosure that has a different user interface. For example, the NS sensor features a dial to adjust the zone temperature setpoint, whereas the TMZ features a pushbutton keypad. As a result, we recommend you work with your customer to help them and their building's occupants understand how to use the adjustment features of the new NS sensor.

When using an FX-PC controller to replace a VAV1xx controller that uses a TE-77xx wireless transmitter/receiver, you must also replace the TE-77xx with the Facility Explorer One-to-One Wireless Room Sensing System. For more information, refer to the Facility Explorer One-to-One Wireless Room Sensing System Product Bulletin (LIT-12011664).

When using an FX-PC controller to replace a UNT controller that uses an M100C zone bus actuator, you must replace the actuator with a non-networked actuator. For dampers, use the M9100/M9200 Series. For valves, use the VA7800/VA-7150 Series.

To control the new actuator, use the available analog output or configurable output interfaces on the FX-PC controller. If none are available, add an FX-PCX Expansion I/O Module.