Control logic configuration - Facility Explorer - LIT-12012045 - Bulb controller - Facility Explorer N2 Controller

Modernization Guide for N2 Controllers - Facility Explorer

Product
Network and Communications > N2 Controls > Facility Explorer N2 Controller
Document type
User Guide
Document number
LIT-12012045
Revision date
22/03/2019
Table 1. Control logic comparisons
Attribute

VAV1xx

FX-PCV1832

Implication

Programming Tool

HVACPro

CCT

Recreate the VAV's control logic with CCT.

Control Logic

Q/A Session for VAV Single Duct

System Selection Wizard for VAV Single Duct

Recreating the VAV's control logic should be straightforward by using the CCT System Selection Wizard or Sideloop Wizard.

Sideloop Session

Sideloop Wizard

Downloading

Locally through the Zone Bus or N2 Bus using AS-CVPRO or MM-CVT or remotely using NAE Passthrough

Locally through SA Bus using FX-BTCVT Bluetooth Commissioning Converter

Must be onsite to download application using CCT.