Room Sensor comparisons - Facility Explorer - LIT-12012045 - Bulb controller - Facility Explorer N2 Controller

Modernization Guide for N2 Controllers - Facility Explorer

Product
Network and Communications > N2 Controls > Facility Explorer N2 Controller
Document type
User Guide
Document number
LIT-12012045
Revision date
22/03/2019
Table 1. Room Sensor comparisons
Attribute

UNT

FX-PCG Controller

Implication

Network Sensors Supported

TMZ Series Zone Sensors

NS Series Network Sensors

Replace TMZ with NS sensor.

Wireless Sensors Supported

TE-77 Wireless Room Sensor Transmitter/Receiver

FX-WRZ7860 One-to-One Wireless Sensing System

Replace TE-77 with FX-WRZ7860 One-to-One Wireless Sensing System.

WRS-TTxx

FX-WRZ7860 One-to-One Wireless Sensing System

Replace WRS-TTxx with FX-WRZ7860 One-to-One Wireless Sensing System.

Analog Sensors Supported

TE-77 and TE-78 Series

TE-77 and TE-78 Series

Reusing sensors is possible.

Note: Some room sensors (TE-6100-11 and -12, TE-67xx, and TE-67xx) featured modular (phone) jack connections and require adaptation for use with the FX-PC controllers.

If you reuse a TE-67xx or TE-68xx series sensor, be aware that the single setpoint or no setpoint models feature an LED, but the FX-PC controller does not support the LED. As a result, you need to change the sensor's DIP switch settings as follows:

  • If Temporary Occupied function is required for the application, set the DIP switch positions on the back of the sensor to down, up, and down (LED disabled, but Sensor and Push Button enabled). The FX-PC controllers do not support the shorting of AI-1 to sense the Temp Occ button.
  • If Temporary Occupied function is not required, set the DIP switch positions to down, down, and down (LED and PB disabled).
Figure 1. TE-67xx and TE-68xx Sensor DIP Switch Setting

Dual setpoint sensor models do not feature an LED. Therefore, you do not need to change the DIP switch settings.