Footprint considerations - Facility Explorer - LIT-12012045 - Field Device - N2 Controllers

Modernization Guide for N2 Controllers - Facility Explorer

Brand
Facility Explorer
Product name
N2 Controllers
Document type
User Guide
Document number
LIT-12012045
Revision date
2019-03-22
Language
English

All models of UNT controllers have a footprint slightly larger than an FX-PCG1611 controller, so replacing a UNT with an FX-PCG1611 using the same enclosure space is highly probable. The FX-PCG2611 is approximately 1 in. (2.5 cm) wider than a UNT. As a result, if you use an FX-PCG2611 to replace a UNT, be sure to verify that enough space is available in the enclosure.

Figure 1. Dimensional comparison of UNT versus FX-PCG1611

Figure 2. Dimension comparison of UNT versus FX-PCG2611

Table 1. Dimensional comparison of UNT versus FX-PCG1611 and FX-PCG2611

Dimension

UNT (All Models)

FX-PCG1611

FX-PCG2611

Height

165 mm (6.5 in.)

150 mm (5 9 in.)

150 mm (5 9 in.)

Width

163 mm (6.4 in.)

164 mm (6.5 in.)

190 mm (7.5 in.)

Depth

56 mm (2.2 in.)

54 mm (2.1 in.)

54 mm (2.1 in.)