Attribute |
DX-9100 |
FX-PCA3611 |
Implication |
---|---|---|---|
I/O Wiring |
|||
Connection Location |
See Figure 1. |
See Figure 1. |
You can reuse the existing I/O wiring if the existing wiring is long enough to reach the FX-PCA3611 I/O wiring connection points. If not, you need to lengthen the I/O wiring. |
Connection Type |
Fixed screw terminal connectors |
Fixed screw terminal connectors |
No change is necessary. |
N2 Wiring |
|||
Connection Location |
See Figure 1. |
See Figure 1. |
You can reuse the existing I/O wiring if the existing wiring is long enough to reach the FX-PCA3611 wiring connection points. If not, you need to lengthen the I/O wiring. |
Connection Type |
4-wire removable screw terminal connector |
4-wire removable screw terminal connector |
Replace the DX-9100's N2 wiring connector with the FX-PCA3611's wiring connecter. |
Power Supply Wiring |
|||
Connection Location |
See Figure 1. |
See Figure 1. |
You can reuse the existing power supply wiring if the existing wiring is long enough to reach the FX-PCA3611 power supply connection point. If not, you need to lengthen the I/O wiring. |
Connection Type |
Fixed, 2-wire screw terminal connector |
Removable, 2-wire screw terminal connector |
No change is necessary. |
Figure 1. Comparison between DX-9100 and FX-PCA3611 Controllers' wiring connection
locations