Display comparison - Facility Explorer - LIT-12012045 - Field Device - N2 Controllers

Modernization Guide for N2 Controllers - Facility Explorer

Brand
Facility Explorer
Product name
N2 Controllers
Document type
User Guide
Document number
LIT-12012045
Revision date
2019-03-22
Language
English
The DX-9100 featured an onboard LCD display and an optional DT9100 display unit. You can partially duplicate the local display functionality by replacing it with an FX-DIS1710. However, the FX-DIS1710 does not provide access to real-time clock functions (such as scheduling, trending, and alarming).
Table 1. Differences between DX-9100 front panel display, DT-9100 local display, and FX-DIS1710

Function or feature

DX front panel

DT-9100 local display

FX-DIS1710

Show attached expansion module points

Yes

Programmable

Yes

Password protection

No

Programmable

Single user

I/O Override capability

LCP Key inserted

Programmable

Yes

Setpoint adjustment

LCP Key inserted

Programmable

Yes

Display Real Time Clock, Calendar, Exception Days, Daylight Saving Time

Yes

Display date and time only

Display date and time only

Adjust Clock and Schedule functions

LCP Key inserted

No

No