Control logic configuration - Facility Explorer - LIT-12012045 - Bulb controller - Facility Explorer N2 Controller

Modernization Guide for N2 Controllers - Facility Explorer

Product
Network and Communications > N2 Controls > Facility Explorer N2 Controller
Document number
LIT-12012045
Revision date
22/03/2019
Table 1. Control logic comparison

Attribute

DX-9100

FX-PCA3611

Implication

Programming Tool

GX-Tool

CCT

You can recreate the DX-9100's control logic with CCT, but it requires custom programming using a different programming tool interface.

Programming Modules

Sequencer

Binary Sequencer

Global Sequencer

 
DX-9100 applications created with the GX Tool cannot be duplicated using the CCT System Selection Wizard. As a result, you must recreate the control application using the CCT custom programming capabilities.