Additional considerations - Facility Explorer - LIT-12012045 - Bulb controller - Facility Explorer N2 Controller

Modernization Guide for N2 Controllers - Facility Explorer

Product
Network and Communications > N2 Controls > Facility Explorer N2 Controller
Document type
User Guide
Document number
LIT-12012045
Revision date
22/03/2019

When using active sensors, be sure that the FX-PC controller and I/O module can provide sufficient current at the voltage required by transmitters.

Current mode of Universal Input range is limited to 4-20 mA. The FX-PC controller does not support the 0-20 mA Analog Input range.

FX-PC controller power requirements are greater than DX-9100. Recalculate power requirements for all replacement configurations. Include any auxiliary devices that are also powered by the DX-9100 or its transformer. Remember to include power requirement for any FX-DIS1710 module when calculating transformer capacity.

The DX family used a slightly different communication protocol. The FX-PC family controllers use the N2 Open protocol.

The real-time clock and alarm functions available in FX-PC controllers support many stand-alone applications.