Zone Terminal Unit considerations - Facility Explorer - LIT-12012045 - Bulb controller - Facility Explorer N2 Controller

Modernization Guide for N2 Controllers - Facility Explorer

Product
Network and Communications > N2 Controls > Facility Explorer N2 Controller
Document type
User Guide
Document number
LIT-12012045
Revision date
22/03/2019

The AHU controller supported an optional ZTU Zone Terminal Unit, which is not compatible and cannot be used with FX-PC controllers. You can partially duplicate the Zone Terminal functionality by replacing it with an FX-DIS1710 Local Display/Keypad; however, the FX-DIS1710 does not provide access to real-time clock functions such as scheduling, trending, and alarming.