Control logic configuration - Facility Explorer - LIT-12012045 - Field Device - N2 Controllers

Modernization Guide for N2 Controllers - Facility Explorer

Brand
Facility Explorer
Product name
N2 Controllers
Document type
User Guide
Document number
LIT-12012045
Revision date
2019-03-22
Language
English
Table 1. Control logic comparisons
Attribute

AHU

FX-PCA

Implication

Programming Tool

HVACPro

CCT

Recreate the AHU's control logic with CCT.

Control Logic

Q/A Session for mixed air single path, mixed air dual path, 100% outside air single path, 100% outside air dual path

System Selection Wizard for mixed air single duct, mixed air dual duct, 100% outside air single duct, 100% outside air dual duct

Recreating the AHU's control logic should be straightforward by using the CCT System Selection Wizard or Sideloop Wizard.

Sideloop Session

Sideloop Wizard

Downloading

Locally through the Zone Bus or N2 Bus using AS-CVPRO or MM-CVT or remotely using NAE Passthrough

Locally through SA Bus using FX-BTCVT Bluetooth Commissioning Converter

Must be onsite to download application using CCT.