Replacing AHU Air Handling Unit Controllers - Facility Explorer - LIT-12012045 - Bulb controller - Facility Explorer N2 Controller

Modernization Guide for N2 Controllers - Facility Explorer

Product
Network and Communications > N2 Controls > Facility Explorer N2 Controller
Document number
LIT-12012045
Revision date
22/03/2019

AHU controllers were used extensively for controlling air handling units, especially for complex units requiring more I/O interfaces than the UNT. Many FX-PC controller models can replace an AHU, but we recommend using the FX-PCA3611 because of its onboard I/O complement. If the FX-PCA3611 controller does not have enough onboard I/O to meet the replacement application requirements, then add FX-PCX Expansion I/O Modules.