Mounting - Facility Explorer - LIT-12012045 - Field Device - N2 Controllers

Modernization Guide for N2 Controllers - Facility Explorer

Brand
Facility Explorer
Product name
N2 Controllers
Document type
User Guide
Document number
LIT-12012045
Revision date
2019-03-22
Language
English

FX-PC controllers are not physically identical to legacy N2 controllers and have a different mounting footprint. As a result, when using FX-PC controllers to replace legacy N2 controllers, ensure that the intended mounting location (for example, if reusing the existing control panel) has enough space to accommodate the FX-PC controller. See Specific device differences and considerations for specific dimensions for legacy N2 controllers and their suggested FX-PC controller replacements.

Note: Depending on the I/O count used on the legacy N2 controller, two or more physical controllers (an FX-PCG/FX-PCX combination) may be needed to replace a single N2 controller.