About this task
When you are ready to move to a BACnet MS/TP configuration, use CCT to switch the FX-PC controllers' field bus network to BACnet MS/TP and then re-download the controller application files (*.caf) to the desired FX-PC controllers.
As you convert FX-PC controllers to BACnet MS/TP, we recommend that you keep the controllers disconnected from the Field Controller (FC) Bus network until all have been converted to BACnet MS/TP and the supervisory controller has been reconfigured for BACnet MS/TP. Follow these steps to convert N2-configured FX-PC controllers to BACnet MS/TP: