Summary of Changes - Facility Explorer - Metasys - LIT-12011999 - TL-MAP1810-0Px - TL-MAP-1810-0Sx - Gateway/Router - MAP Gateway - 5.1

Mobile Access Portal Gateway User Guide

Product
Network and Communications > Gateways and Routers > MAP Gateway
Document type
User Guide
Document number
LIT-12011999
Version
5.1
Revision date
2022-11-03

The following information is new or revised:

  • Added a note to Software Updates in Table 1
  • Updated MAP Gateway UI and Navigation to include a change to the domain in the MAP Gateway User Interfaces uses, new logout button, and ad hoc live trends added to the navigation menu.
  • Updated Main Menu to include new point in Device and Point Checkout. Added new points Box flow test, Unattended Download.
  • Updated MAP Settings Menu Descriptions to include two updates to the Wi-Fi Settings and information on Site Append menu option.
  • Added new section - Appendix: Turning off the Wi-Fi.