Appendix: Turning off the Wi-Fi - Facility Explorer - Metasys - LIT-12011999 - TL-MAP1810-0Px - TL-MAP-1810-0Sx - Gateway/Router - MAP Gateway - 5.1

Mobile Access Portal Gateway User Guide

Brand
Facility Explorer
Metasys
Product name
MAP Gateway
Document type
User Guide
Document number
LIT-12011999
Version
5.1
Revision date
2022-11-03
Language
English

About this task

Note: Before turning the Wi-Fi off, you must ensure that the Ethernet is turned on. Failure to do will require a reset of the device and potential loss of stored settings and data.

Procedure

  1. Refer to the Mobile Access Portal Gateway Network and IT Guidance Technical Bulletin (LIT-12012015) for connecting the MAP through Ethernet.
  2. Once you have enabled Ethernet, identify the device IP address by navigating to the Main Menu > Device List and then back to the MAP Gateway > Settings > Ethernet.
  3. Go to the settings tab, Wi-Fi access point.
  4. Select the Disable Wi-Fi box.
  5. Exit Settings.
  6. Initiate the log in process again, through a laptop Ethernet Port.