If you forget your password, or you want to restore the unit to factory defaults, the MAP Gateway offers two reset functions: a Network Reset function that only resets Wi-Fi and Ethernet settings, and a Reset to Factory Defaults function that resets all unit settings (including user profiles). Reset to Factory Defaults also replaces the device's SSL certificate with the Johnson Controls® self-signed certificate that was configured in the factory.
The Network Reset function is intended for users who forget their Wi-Fi connection information. The Reset to Factory Defaults function is for use by administrators who may want to clear all configured settings from a device, including all user profiles. For information on resetting the unit, see Table 1.
The reset button is embedded into the back of the MAP Gateway housing so that it cannot be activated by accident. Use a small screwdriver or similar tool to press the reset button.
Before attempting either of the following reset functions, apply power to the MAP Gateway and wait until the Fault LED stops flashing.
- If you are connected to the network when you press the reset button, you are disconnected.
- If you press the reset button for more than 9 seconds, or do not confirm the reset, the reset operation is cancelled.
- If a fault condition already exists, the reset button is disabled.
Reset Function |
Reset Operation |
---|---|
Reset Only Wi-Fi and Ethernet Settings (Network Reset) to Factory Defaults |
Do not cycle power. The LEDs may continue to flash until the MAP Gateway resets and returns to normal operation. The Wi-Fi and Ethernet settings are reset to factory defaults. Use the Default SSID and passphrase to connect to the MAP Gateway, and then login to reconfigure all the required settings. |
Reset to Factory Defaults |
Do not cycle power. The LEDs may continue to flash normally until the MAP Gateway resets and then returns to normal operation. All unit settings are reset to factory defaults. Use the Default SSID and passphrase to connect to the MAP Gateway, and then login using the default User and Password to reconfigure all the required settings. |